RadarGUI v2.0.0 (June, 2020) ================================= General New Features: ===================== - Enhanced firmware flashing feature to support both 24GHz/60GHz devices * User needs to install Segger JLink on PC to flash 24GHz devices - Logging tab introduced to assist GUI for bug reporting. User can; * Enable/Disable logging * Save/Clear Logs * Select between five log levels - New visualization plots and views added for few devices; * FFT magnitude tracker * Motion tracker * Direction of motion tracker * Polar plot with segment highlighting * Range plot with zone highlighting and single target tracking - Renamed Revert button to Cancel for all perspectives in Settings pane. - Make Labels next to icons in toolbar clickable 60GHz Features: =============== - Updated the Radar SDK dll to version 2.0.0 - Segmentation application support added with; * Polar plot with maximum three segments visualization * Configuration view for segmentation algorithm parameters * Recording and playback of segmentation application output * Save/Load parameters to/from JSON file - Added ADC expert settings in standard mode * Sample rate (kHz) * ADC Tracking * Sampling Time * Double MSB Time - BGT60ATR24C device support added with; * Standard Mode view * MIMO configuration * Save/Load parameters to/from XML file * Recording and playback feature * Visualization plots - Time and Frequency domain plot - RangeDoppler plot * Note: No SDK applications supported with this device - BGT60LTR11 (Doppler based Motion Detection) device support added; * System Settings provided to select - Mode (Continuous or Pulse) - Pulse parameters - TX Power and RX IF gain control - Motion Sensitivity * Save/Load parameters to/from XML file * Recording and Playback feature * Visualization plots - Time and Frequency domain plot (Continuous mode only) - Motion Tracker and Motion View - Direction Tracker and Direction of Movement view 24GHz Features: =============== - Sense2GoL Software Controlled FMCW (BGT24LTR11) device support added; * Range plot with zones and target highlighting * Configuration view for device and DSP settings * Recording and playback feature * Visualization plots - Time domain plot - Target Signal Strength Tracker - Motion Tracker and Motion View - Direction Tracker and Direction of Movement view Bug Fixes: ========== - Frequency domain plot stopped showing results for 64 samples per chirp selection for 24GHz devices - Default button did not reset the values for 24GHz devices - Recording to raw binary format more than 1000 frames is missing frames on playback - Chirp selection was visible in context menu of time domain plot for pure doppler device - Metric selection and User Mode was enable in Settings menu for 60GHz devices - Opening multiple instances of the same plot shows wrong info on the previous instance Known Issues: ============= - On slower PCs, Tracker plots get laggy sometimes. Following workarounds can be applied; * Reduce the frame rate from toolbar or frame rate slider * Increase GUI refresh rate period from Settings->Advance menu