2020-09-23 V1.7 -Update SP49_InterfaceBoard_Library to V1.7 -Update included board FW to V1.5 -Add feature to average multiple acquisitions in mode "normal" -Modified position of label when a marker-line is plottet and added circle to point at the marker-line 2020-06-18 V1.6 -Added possibility to send also binary-encoded data in LF-telegram (enter in format e.g. 0b1010) -Added possibility to use also edges of logical pin levels for current-measurment trigger 2020-03-19 V1.5 -Update SP49_InterfaceBoard_Library to V1.5.2 -Fixed rendering of markers was not arranged correctly at some conditions -Fixed wrong calculation of sampling-time for current-measurement, resulting current-measurement could sometimes not be started 2019-12-02 V1.4 -Added feature to stream also logical levels of PP2/PP3 during current-streaming 2019-08-20 V1.3 -Bugfix for auto-firmware-update of board -Minor improvements -New firmware of board included -Bugfix for carrier-generation (chip-times were sometimes wrong) 2019-07-23 V1.2 -Added version check of board FW -Fixed that "Inverted Manchester" checkbox did created inverted coding -Use updated interface-library for SP49 development-board 2019-07-05 V1.1 -Initial release for customers